Other Parts Discussed in Thread: LM5160
Tool/software: WEBENCH® Design Tools
Hi,
I am using this converter on my design for genarate an isolated 5V/1.5A with input voltage range of 20V-65V.
Before I was choose this one, I was check the device by webench:
https://webench.ti.com/power-designer/switching-regulator/customize/149
I Used "LM5160 QuickStartCalculator - FinalVersion" calculator of TI (that show I can reach only 1.2A that OK too) and calculate by my self according to the datasheet of the device for make sure the device will stand by the requirments and everything was OK.
In those days the design arrived, start to check it and I have a problem that when I put load that consume at least 200mA on the secondary side (the isolated one), the level voltage is falling to 4.5V (10%!!).
the deferent between webench and my design is:
- instead Cout i put a 33uF polymar tantalum capacitor (T543X336K050ATW040)
- instead Cout2 i put a 330uF polymar tantalum capacitor (T530X337M010ATE006)
- instead D1 i put MBRAF3200T3G
While I continue to check the circuit and trying to find the problem, please your help in this problem.
hope for fast and useful answer :)
BR,
Itzik