This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: BQ24650

Part Number: BQ24650

Hi

BQ24650 application circuit as below.

Electronic load connect to output, electronic load mode is set to power mode when power greater than 0.5 W, BQ24650 output are powered down until the electronic load set up as the voltage mode (Analog Switch/Multiplexer (less than or equal to 5V) charge of a battery) is about 85% efficiency.

Bq24650 charging module is followed by the need for lithium ion battery and parallel the second DC/DC power circuit.

When the battery is not connected, directly connect the DC / DC load, the bq24650 will also be powered off and cut off.
 Does we can connect the battery and parallel DC-DC load.

Thanks

Star