This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51013: Questions about wireless reveicer and battery charging

Part Number: BQ51013B
Other Parts Discussed in Thread: BQ24040, , BQ24072

Hello, sorry for quite beginner questions, but could you please help me out with these?

I am thinking about wireless receiver + Li-Pol charger for my project. I will have small two-wired 270mAh Li-Pol battery without NTC and I need to be able to charge while also powering my device.

I have already been searching quite long for something and found the BQ51013B Qi receiver and the BQ24040 charger. Are these ok for my needs? I have never dealt with charging circuits before so I rather came to ask.

Also I am slightly confused by your terminology in the BQ24040 datasheet - there is written about "fast charging" - is it just the TI's terminology for normal charging? I have always thought about "fast charging" as of for example Qualcomm's quick charge so.. But I believe your "fast charging" is like normal charging for me, right?

But to my very main questions:

  • I should limit charger's output current to battery, right?
  • Can I just pull the BQ24040's ISET2 to High without worrying about anything?
  • Should I take care of anything else I didn't mention here?

Thank you in advance!

It's really just my hobby project for learning something new so if something fails, it will not cause anything to anyone.

  • Hello,

    If you need to be able to charge and power your system at the same time, you might look into BQ24072 family of devices which has powerpath. 

    I am not sure if fast charging is trademarked but typically I have seen fast charging being mentioned when >1C of charge current is being pumped into the battery itself. 

    A powerpath device will be able to control the precise amount of current going into the battery independent of the system load. On a non-powerpath device load transients can vary the actual charging current- great for applications being dropped into a cradle while system consumes very little current if any- 

    Regards,

    Gautham

  • Hello,

    Let us know if you have any questions on this thread. 

    Regards,

    Gautham