Hi Team,
One of my customer using this device have below query during over current operation. Please help with output voltage to output current graph (Or Input v Output current)
If the load draws 3.5A< Iout < 6.8A, will the Regulator go to frequency fold back mode due to the current limit or go to thermal shutdown?
Is the max current defined for max output voltage?
Also datasheet mentions open loop current limit is 6.8A max. What is the closed loop current limit?
Please help with your comments and inputs. Thanks in advance for the help and support.
Regards, Shinu Mathew.