This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS568230EVM: Spur detected on device upon cold-crank but recovers upon increased load with device under FCCM mode

Part Number: TPS568230EVM
Other Parts Discussed in Thread: TPS568230

Hi,

We have some questions with regards to the evaluation of TPS568230 while evaluating the TPS568230EVM. 

As of now we have TPS568230 operate in FCCM mode with Vin 7.5V & Vout 3.6V tested on EVM & we've observed the following outcomes. Hence will need advise on

  • end equipment started with non-transmit mode @ Iout ~200mA & spur was detected
  • end equipment begin to transmit with output load @ Iout ~1A, device operate without spur. So we would like to know if this is normal behavior of this device?
  • additionally are there any conditions required to meet so that such occurrence can be avoided?
  • we also bbserved ~1MHz of switching frequency @ Vin but output is normal, what may be the potential root cause?

Additionally are there any app-notes with regards to DCAP3 technology which we can read on? Thanks.

Regards,

Leo