This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I can´t import the LMZM33602 part on Mentor Xpedition. I've used the *.bxl file and the Ultralibrarian. Could you send me a video with the process? Thank you.
Hi Jessica,
I'm not sure if you are aware, the system has two posts created under your username as shown below unless I've mistaken the original questions:
Please help clarify if these are indeed duplicate post or do you have another issue with the LMZM33602?
In order to consolidate the troubleshooting, I would recommend we close this thread and stay on the second thread mentioned above instead of having multiple threads with the same question opened.
Regards,
Jimmy