Hello E2E team,
I have a question and I hope you bear with me. I am planning to control the input voltage of LM20343. The only modification is to connect the voltage divider to sense the input voltage, not the output voltage. At the input, I plan to connect a solar PV panel while at the output I will connect constant voltage load (for example: a load whose voltage is always 10V). Constant voltage load is achieved via a DC electronic load. Now, can I control the input (solar panel) voltage in this case? this is my question and I also attached a demonstration photo for it.