This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPIC74100-Q1: Over-voltage and over-current safety protection

Part Number: TPIC74100-Q1

How can over voltage and over current protection be done with this IC?

  • Hi Aladdin,

    the device internally set to 5V. there is no FB pin to change the VOUT. thus it doesn't required output over voltage protection.

    The over current is protect by the internal MOSFET Q1. the Q1 will turn off if the inductor peak current reach 2A.