About D+/ d-detection,
USB Host or Charging Port D+/ d-detection Compatible to USB Battery Charger Spec (BC1.2)
1. How long will it take to start D+/ d-detection after plugging into the USB
2. How long will each D+/ d-detection last?What interactions did you have?
3. After the first D+/ d-detection, is it possible to conduct D+/ d-detection again and again? How long is the interval?What is the frequency?
4. Whether the D+/ d-detection of BQ24295 will be affected if BQ24295 is connected with the D+/ d-chip of bluetooth?
5, when plugged into the computer USB, how to set to ensure that the output charging current is 500mAh, not 200mah or lower.