This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
if the input is less than 42V, we have LM25180 for this application. The 1K price is less than LM5180.
Thanks
In this design transformer limiting the current up to 60mA. Can we connect directly the voltage output from the transformer to TPS26 Vin rather than using Jumper J1?
Kindly explain the purpose of Jumper J1 and J2
Hi
sorry, I only charge of LM5180, I will help forward this question to related support team, they will help on your question of TPS26625.
Thanks
Hi Dheeraj,
Apologies for the delay. These jumpers are placed to facilitate individual block testing.
Yes, you can directly connect the voltage output from the transformer to TPS26625.
Best Regards, Rakesh