Tool/software: WEBENCH® Design Tools
Hello,
on the Demoboards and in the Webbench Designer TI recomments for the Cboot-Capacitor Parts with max. voltages from 10V to 16V. All Designs work with Inputvoltages greater 20V
The Cboot is connected to the SW-Output. At the SW-Output you measure voltage differences from appoximately the Vin-Voltage, >20V.
Questions:
Which max. voltages do you measure accross Cboot ?
Should the max. voltage for the CB-Capacitor be greater than the voltage of Vin (example 35V or 50V) ??
Kind regards
Manfred