Hello,
I'm slightly confused on the channel to channel current error spec. The datasheet describes it as +/-7%, but based on the provided equation it seems like the difference between out1 and out2 could be 14%:
If I have Iave set to 10mA, then one channel could be at 9.3mA and the other could be at 10.7ma, making the difference 14% between the two. Is my understanding correct?
Thanks,
Michael