This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22959: Parallel connection available for High Load Current.

Part Number: TPS22959

Hello

The customer is considering a load switch at 20A load current.
The load current of TPS22959 is up to 15A.
Can it be used up to 20A by connecting in parallel?

Best Regards.

  • Hi,

    Welcome to E2E!

    When using load switches in parallel the overall current capacity is increased. Since the TPS22959 has a capacity of 15A, connecting 2 in parallel will allow the load switches to support the 20A load current.

    Let me know if you have any additional questions,

    Best regards,

    Andy Robles