Hello,
I had a question concerning the output current of the TPS76901-HT device. I know the maximum rated current is 100mA, but the DS says the current limit is 505mA at 210degC. Do you have any information on the change of output voltage when the load current increases from 100mA to 500mA? I am assuming the voltage folds back but want to know how the voltage behaves (especially between 200mA-300mA).
Thank you,
Brandon