I'm sorry my poor English.
I've evaluated LM5160. But Output voltage is very weak and unstable.
ref. datasheet P23 Fig.28
---my circuit---
Input=12V, Output=5V
my component
R6=100k
R10= 20k
R7=200k (RON)
If R7=100k, Output voltage is more weak and unstable.
R8=7k
R9=2K
C13=0.047uF
R4=15K
C9=0.1uF
C10 = 47uF (Ceramic capacitor)
C11 = 330uF (Electrolytic capacitor)
T1=750314597
C1 = 47uF (Ceramic capacitor)
C2 = 330uF (Electrolytic capacitor)
If I connect 100Ω to J1, Output voltage become 3.5~4.0V.
If I connect No load to J1, Output voltage become 6V over.
I would like to generate 5V as output voltage.
Why is Output voltage as LM5160 weak and unstable in my circuit?
Please give me advise.
Best regard.