Other Parts Discussed in Thread: BQ76920, BQ76930, BQ76940
I'd like to use BQ77915 for our product as internal battery protection. After shipment from our factory, load connected to BQ77915 can NOT be removed.
Could you let me know how to disable Load detection as recovery method from UV,OCD,...
In our test, once some fault occured and DSG FET is turned off, we can't turn on the system.
I'm considering about 2 ideas.
1) Change R_LD and then VLD keeps under VLDT
-> If OCC fault occurs, is it impossible to recover ? If we assume OCC will not occur because OCC threshold(20A) is much higher than charge current (1.5A), 1) is useful solution ?
2) Remove CHG FET and DSG FET. Connect CHG pin and DSG pin to MCU.
If the MCU detects fault state of BQ77915, then MCU reduces system current or stop charging or etc.
I had seen other questions in E2E and I found BQ7791504. Is it better to use for our product ?