Other Parts Discussed in Thread: BQ77905
Hello,
I have been having issues with trying to reset an over current fault with the BQ77915. Is removing the load the only possible way to reset the fault? This is not possible for our use case, so Ideally there would be another way to reset the fault. Connecting the battery charger is also not always possible for the product that this chip is being used for.
I tried using the BQ7791504, since that was recommended in a similar forum post to this one. I replaced the IC that was on the EVM with the BQ7791504. This ended up causing the overcurrent protection feature to not work at all, and I was able to draw a significant amount of current from my battery. This is not ideal, along with having the temperature sensing features disabled for the BQ7791504.
If removing the load is the only way to reset this fault, is there a similar TI chip that does not have this "feature"?
Regards,
Alex Mazur