Other Parts Discussed in Thread: TIDA-010062, TIDM-1007, TIDM-02008
Hello,
We are trying to implement Bi-directional 3-phase Controlled rectifier + PFC. Bi-directional where input can be provided to the DC side or AC side & Controlled where DC side can vary from 48 to 400VDC. Further, we prefer to use the new GaN power switches.
Designs & Questions
* TIDA-00961 (GaN). If this design is adapted to three-phase we will realize the PFC sought. It seems that this design does not allow controlling the DC voltage level. We have been advised (by TI senior engineer) that this design would not support 48VDC, only 400VDC with much voltage ripple
Questions;
- What is the ripple level as percentage of the output DC volt?
- The design produces 400VDC. This is a controlled GaN rectifier and further has two controlled MOSFETs. For sure the system has enough degrees of freedom to control both DC output and power factor and hence we must be able to reduce that DC volt output as well as PFC? What would be the minimum DC level that we can realize? And why cannot we have full control over the DC range.
- Why have not we used GaN switches to replace the auxiliary MOSFET switches.
- Is this design bi-directional? Can we supply 400VDC and get AC output?
* TIDM-1007 (GaN). This design is very similar to TIDA-00961.
Questions;
- The location of the auxiliary MOSFETs has changed as compared to TIDA-00961. What does it do?
- Do we get higher or lower DC voltage ripple as compared to TIDA-00961?
- Does this design generate three phases out of a single phase? If so are these 120degrees phase shifted? If so why do we do that?
- Same 4 questions posed for TIDA-00961.
* TIDA-010062 (GaN). This is a two-stage design PFC à DC-DC.
Questions;
- Is this design bi-directional? Can we supply 400VDC and get AC output?
* TIDA-00951 (no GaN). This is a design that allows 48VDC 400VDC bi-directional
Questions;
- Would you recommend using TIDM-1007 + TIDA-00951 OR TIDA-010062 to realize the target listed above (ie bi-directional controlled rectification +PFC)
- Does TI have any reference design that realizes bi-directional 48VDC-400VDC using GaN?
Regards
Sam