Dear all,
Thank you for your reply.
I would like to ask about application circuit of datasheet.
The TPS61085 data sheet describes the following application circuit and states that Iout can flow up to 600mA.
However, when Iout(max) of the above application circuit was calculated using the Iout(max) formula described in TPS61085, it was 0.467A.
(Calculated assuming 100% efficiency)
Is this okay because the application circuit on the datasheet is wrong?
*By the way, the calculation conditions are as follows.
Vin=3.3V
Vout = 12V
η=1
Furthermore, Duty and ΔIL are as follows.
Duty=0.725
ΔIL=0.60417