Hello. I am developing a board in which I use bq24030. Reading the documentation, I can’t understand why when I connect usb 5.0 V, I get 3.7 V output. Tell me why and how to regulate it? (The battery is not connected. There is no load.)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello. I am developing a board in which I use bq24030. Reading the documentation, I can’t understand why when I connect usb 5.0 V, I get 3.7 V output. Tell me why and how to regulate it? (The battery is not connected. There is no load.)
Hello,
Can you try using another voltmeter. I would expect switching to polarity to give you negative of initial voltage.
Also if you have 5V on input, you should have around the same on OUT. What resistor do you have on DPPM
Hello,
You should be able to order new ones online through your local vendor.