This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG3410R050: Layout modeling problem of LMG3410

Part Number: LMG3410R050


Hello,
Recently selected the LMG3410 device, and now encountered a problem in PCB design modeling.

LMG341xR050.pdf

In the data sheet, there is a large PAD on the bottom of the device.

I don’t know whether to build a complete large PAD according to the recommended 27 pages of the manual when building the PCB pad, or build the PAD into 10 small ones as recommended on page 35 of the manual. PAD?


The third page of the manual says that connecting the PAD to the source through the via is not necessary to connect the source to the source through the via in the middle layer.

It is not possible to directly connect the PAD to the source of 12-16 and 18-24 during modeling Connected?

Thank you.