This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21520-Q1: About NC pin

Part Number: UCC21520-Q1

Hi,

Customer wants to connect pin 12 and pin 13.
(The two pins are connected but floating.)
The reason is to reduce the number of pin probe tests in the application.

Is it OK to connect pins 12 and 13?
If it is NG, please tell me the reason.



Regards,
Yusuke



  • Tsukui,

    So long as NC pins are floating and creepage and clearance from ch-A to CH-B are maintained, you may short the 2 as there no internal connections according to Section 5 of datasheet.

    Regards,

    -Mamadou