This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I am using the simulation model of LM337 in LTSpice. As a circuit, we would like to apply an offset voltage to GND to a standard circuit and raise the output voltage by the offset voltage. However, perhaps the provided model did not give the desired result because the internal reference voltage was fixed.
Is there a model in which the reference voltage of the LM337 is not fixed?
Beat Regards,
Tom Liu
Hi John,
I confirmed by simulation again, but even if the offset voltage was given, the output did not rise higher than 0V in the positive direction. As for usage, we would like to use it as a suction-type +1.3V power supply. Of course, we understand that the data sheet states that the output voltage range is negative voltage only. Does it mean that the simulation model does not support the above behavior because it is out of rating?
Beat Regards,
Tom Liu
Hi John,
In your result I also saw Vout is lower than 0V. Can Vout be higher than 0V?
I attached the simulation circuit and the result. Vout is monitored by DC sweeping V4 to the circuit of -5V input and -2.5V output. In the attached figure, Vout is 0V and has reached the ceiling.
Beat Regards,
Tom Liu
Hi Tom,
The LM337 can only sink current from the highest potential. I see the issue you are having with the model now and it is likely an issue whether you use TINA or LT Spice, the model internal has a '0' or GND reference.
Can you order an EVM to try this on the bench? If not, I can help you to order one if you provide your contact details.