Hi TI Team,
I have a question about TPS2412 and please checks my customer application.
"Can be the TPS2412 Vdd powered form A as the red make?"
My customer found the IC broken of the gate PIN, there is no single after the function.
After A-B-A the PCBA can be work with a good IC.
The information as the blowing:
Topology: Flyback
Application: 12V
Check output overshoot voltage=13.2V
Check OVP voltage=14V
If need more information please feel free let me know, thanks
Customer SCH