Hi
Attached the schematic as below:
The query is when connected load, the first series' voltage is about 100mV lower than the other two series.
Before discharge the voltage detect is the same.
Please give some suggestion.
Thanks
Star
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Attached the schematic as below:
The query is when connected load, the first series' voltage is about 100mV lower than the other two series.
Before discharge the voltage detect is the same.
Please give some suggestion.
Thanks
Star
Hello Star,
Usually when there is a drop between cell voltages under load it means you have interconnection resistance between the cells. Make sure your connections are secure, then add thicker connections between cells if the problem is still occurring.
In some cases it could be a bad battery cell as well.
Sincerely,
Wyatt Keller