Hello,
I am now evaluating Dimming performance and have some problem.
My error might be equivalent to following case but there is not solution so Let me add this case.
"LM3445: Low dim level issue using"
I am using equivalent diagram as Evaluation Board and Valley Fill Capacitance is 10uF each and Trans value is 1.6mH.
At the region when valley fill change series to parallel connection, LED flicker is occurring like as following.
Isw peak is changed from 25mA to 7mA around this Error state.
I guess, there is a little light Jump-up around this region at normal state.
Is there any way to improve this error ?
Kind Regards,
K Sakai