Part Number: UCC28780
Other Parts Discussed in Thread: SN6505B, UCC24612
Ulrich:
seems it is likely my last post did not get posted correctly..
Her eit is
So we are full speed in installing all parts...
BUT!
Ours are all GaN.
See attached TI document using NV6115/6117( do not know why upper one is 6115...it has higher Rds ON...other than that it is exactly the same as 6117)
The document uses NV6117 VDD output to bias the upper isolator & the boost cap.
The Vdd is only 6V & can deliver max 3 mA, plus cannot use the zeners ... with drops remaining uncertain...but certainly ok for eval purposes.
I do not know if a start-up will be guaranteed in this circuit.
See the attached ppt for our scheme. Stiff bias sources are used but I am wondering about start up for different reasons.
Basic differences are
- we use TPS7A2450DBVR to start the bias for the ISO7710 chips and stay with the auxiliary winding generated voltage up to steady-state guaranteed 5V operation.
- We use NV6117 VDD only for the lower isolator
-the auxiliary output powers the lower 6117 throughout because it can handle up to 30V or so.
So the concern is the LDO behavior as the auxiliary starts up from the first 3 pulses...which powers the controller side of PWML. Will it work?
Do you see other start-up issues in our circuit?tidrvm3b28780scheval_DIODES.pdfucc28780startup_gnmr.pptx
We certainly plan to go in steps of HV ...looking out for the white smoke from the chimney....in the end...
-robin4336.tidrvm3b28780scheval_DIODES.pdf4666.ucc28780startup_gnmr.pptx