This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53353: Vreg

Expert 4486 points
Part Number: TPS53353
Other Parts Discussed in Thread: TPS53355,

From the datasheet, it appears that the Vreg pin should be 5V and will start ramping up when the input voltage is above 2V and is independent of enable pin shown in the graph below. 

I am having problems with the Vreg not trying to ramp before the enable pin as shown below. 

 _