Other Parts Discussed in Thread: UCC27282,
Dear Team,
Here is Kevin from Delta Taiwan team.
Do we have high low side driver with a maximum 5V rating here?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kevin,
Thank you for the interest in TI half bridge drivers. It looks like you are looking for a 100V class half bridge driver with lower UVLO, targeting close to 5V operation.
TI does have a recent released device with improved performance over the UCC27200 including lower UVLO voltages. The UCC27282 is a similar function half bridge driver as the UCC27200 with a maximum VDD UVLO of 5.4V. The datasheet for the UCC27282 can be found at the link below.
Confirm if this addresses your questions, or you can post additional questions on this thread.
Regards,