This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you please recommend a part for a buck-boost converter for a battery powered design with the following specifications:
VIN - 2.2 to 5.3 V
VOUT - Fixed 3.3 V
Load current - <500 ma
Efficiency - High
Quiescent Current - Very low. The load (transceiver) will spend most time sleeping and during this time the current drawn.should be minimum possible.
Capacitor Leakage - Minimum (recommendations?)
Thanks and kind Regards,
Sudhir Gupta
Hi Sudhir,
the TPS63900 is closed to this application, please have a look at this device.
Hello Jasper,
TPS63900 seems much nicer and is just what I am looking for. Since my design is a fixed 3.3V output, can I simply use the front page schematic from the data sheet, or will kindly recommend changes to it?
Kind Regards,
Sudhir
Hi Sudhir,
yes, and you can refer to the page 15 to select the resistor value for this device.