Other Parts Discussed in Thread: BQ8015, EV2400, BQ40Z50-R2, ADVANCED-BQMTESTER, BQPRODUCTION, BQMTESTER
Hello
I would like to use alternative for bq8015. What would you recommend? I would like to use it to build EV2300.
Thank you
Go
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I would like to use alternative for bq8015. What would you recommend? I would like to use it to build EV2300.
Thank you
Go
Hello Go,
EV2300 is obsolete. Based on your comment, I think that you are trying to build an EV2300. If that is the case, then there is no drop in replacement available for bq8015. A number of components on the EV2300 are obsolete and not available. I recommend that you use the EV2400 instead.
If you are looking for bq8015 as a gauge, i do not think that there is a pin to pin compatible version that you can use. I would recommend the bq40z50-R2 for replacing an application that previously used bq8015. bq40z50-R2 has lower BOM count and better accuracy.
Regards,
Hello Go,
Please create a separate thread for new questions.
BQMTESTER and ADVANCED-BQMTESTER are not expected to be compatible with EV2400. EV2400 is newer than ADVANCED-BQMTESTER.
BQPRODUCTION is not designed for Windows 10 but is likely to work on Windows 10.
Regards,