Hi all,
The continuous load current of the buck converter is written on the datasheet, I wonder how much limit of peak current that the device can survive?
For example, LMR23630-Q1 device can make continuous 3A.
However the peak current is over than 3A(3.5A ~ 4A depending on the inductor size), how much the limit of the peak current that device can survived?
It's not shown on the datasheet.