This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3823: Short Circuit Current rating

Part Number: TPS3823

I am using TPS3823-25. RESET pin is also connected to JTEG port and during the programming , it will be pulled low. This will create a short circuit on RESET pin of TPS3823.

if I see the spec of TPS3823-25, the short circuit rating is 400uA. So whether I need to use a current limiting resistor at the output of TPS3823. What should be the resistor value ?

also whether this 400uA is for -40 to +85C or for room temperature ?

Also whether any pull down is required at the RESET pin for keeping the RESET output low below 1V supply ?