This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5119: Soft-Start Capacitor Inquiries

Part Number: LM5119

Hello.
I have an inquiry about using the LM5119 from a customer.
In the datasheet, if you look at the tss calculation formula of the Soft Start Capacitor, the Css value of 0.047uF is applied.

1. I am trying to apply a Css value of 0.027uF, is there a problem?


2. And, please let us know if there is an applicable range (Min~Max) of Css capacity value.


3. Finally, when Css is applied to 0.027uF, is there an expected side effect?


please answer about my question.
Thank you.