Tool/software: WEBENCH® Design Tools
Hi.
I have the following design from Webbench:
When implemented on our PCB, I cannot get it to be stable.
In plot below the lines are as follows, the input voltage is 12V 3Amp max, load is 3x4K ohm -> 30mA
Yellow: input voltage
Green: input current (wrong scale)
Red: Switching output
Blue: negative -40V (DCDC output)
Can anybody see any clear reason for the instability?