Other Parts Discussed in Thread: TPS23861
Tool/software: WEBENCH® Design Tools
Dear sir.
When PoE_PSE output voltage higher AC/DC adapter,
Step 1: plugged in PSE first.
Step 2:then an AC/DC adapter plugged in later.
In step2, Why PSE still power on and supply voltage to PD?
Step 3: AC/DC adapter unplugged.
It damaged PD controller TPS2373-4RGW.
We damaged 3 Viking(project name) units in this scenario.
Please help to provide the solution.
Adapter ORing: Viking unit is option 2.
Option 2 applies power between the TPS2373 PoE section and the power circuit
APD pin voltage is 3.2V when AC/DC adapter plugged in, in Viking unit.
TPS2373 specification:
When a voltage of more than about 1.65 V is applied on the APD pin relative to RTN, the
TPS2373 does the following:
• Internal pass MOSFET is turned off
PSE TPS23881EVM and PD TPS2373-4 EVM are also have this issue.
Thanks!
Inventec Appliances Corp.
Steven Kang