Dear TI Team,
while testing our current prototypes, some electrical components on our PCBs got damaged in consequence of volatile power supply voltage (slightly moving lithium ion battery in the device case)
The destroyed (analog) hardware components are powered by the +-5V power rail. This power rail is built up by the TPS65133. This event is reproduceable by switching the Power supply on and off randomly in fast combinations. Please find the oscilloscope print in attachment.
- Vbat (green) = is our main power supply and input for TPS65133
- 3V3 (yellow) = is the logic supply (e.g. the MCU which enables the TPS65133)
- V5v0P (red) = is the positive output of the TPS65133
- V5v0N (blue) = is the negative output of the TPS65133
You see that the positive output (red line) of TPS65133 reach 8V and more. This destroyed some components.
The negative output looks good, because of the constant Off-Time Control.
What do you think about?
Best regards Martin.