Other Parts Discussed in Thread: LM22680
Hello,
I have used the model in LTspice.
In normal operation the model works very well.
Now I wanted simulate the device as an inverting buck-boost converter according to snva856a.pdf chapter 5.
But this does not work.
After some searching I found out, that a "normal" simulation does not work, if the simulation GND is not connected to the GND-PIN, but somewhere else in the network.
Apparently in the simulation file the network "0" is used as absolute GND and is not assigned to the GND PIN of the device.
How can I correct this? (Search " 0 " and replace with " GND " doesn't work.
So you don't need to connect anything to the PIN GND or PAD in the simulation - the circuit still runs in the simulation, but only in a "normal" buck-simulation referred to simulation-GND
B.R.
Wilfried