Other Parts Discussed in Thread: INA139, TLV4333
Hello,
I'm looking for some assistance troubleshooting a TPS65279 circuit that seems to keep going into OVP or OCP whenever it is attached to a load.
When no load is attached it operates as expected (swings to VIN at the output). When the load is attached (in this case a diode load Vf = 2.5V) the output never seems to rise above 1.5V, and no current flows.
I decided to scope SS pin (yellow) and VOUT (blue) and you can see the behavior here:
Since the OSC is 1MHz, (1us cycle) What I believe im seeing is the 512 us cycle hiccup wait time followed by the 16384 us shutdown/restart hiccup time. That would be an overall period of 16896 us (16.896 ms) or the roughly ~17ms im seeing here. I've been reviewing Section 8.3.7.2 Low-Side MOSFET Overcurrent Protection in the TPS65279 datasheet and it specifically mentions that the output overload condition is measured by the COMP pin.
My COMP pin never seems to rise above 75mV, also indicating a overload condition. I took note that my RLIM is set to 7.26A (61.9kOhm) for this channel, and I see that datasheet notes the I_LIMITLSx low-side sink current to be -2.6A, but I do not see what the low-side *source* current limit is.
The sensing feedback circuitry uses a high side current monitor (similar to the INA139), a unity gain op amp buffer, voltage divider (for V_fb) and a voltage DAC. Since there is negligible output current from the TPS65279, the output of the divider never reaches the 0.6V reference voltage.
Any direction would be appreciated.