This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2543: Current Limiting Function

Part Number: TPS2543

Hello team,

My customer has questions about TPS2543 of current limiting function.

Can your team answer the below questions?

  1. By setting CLT1 shown in Table 3 to Hi and CLT2 to 3 to Lo, the DCP_Shorted mode is set, can TPS2543 switch the current limit value with the ILIM_SEL pin?
  2. When the EN terminal and CLT1 terminal are Hi and the IN-OUT is ON, is backflow prevented when an external voltage is applied to OUT?
  3. According to the calculation formula (data sheet P31), the current limiting function of this IC can be limited with a variation of less than ± 10% in the current limit of 500mA to 1.5A. Is this recognition correct?

Best regards,

Shotaro