This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I find there is a minimum on-time(about 200ns) for the LM3445.Min Ton matter means we have worse line regulation spec when TRIAC level is min.
Because Min ton is fix,LED voltage tolerance also effect min Iout.How to achieve constant Iout against Vin Vbuck Vout.
Hi gz,
The maximum switching frequency attainable is limited only by the minimum on-time requirement (200 ns). Worst case scenario for minimum on time is when VBUCK is at its maximum voltage (AC high line) and the LED string voltage (VLED) is at its minimum value.
This is a normal phenomenon for the switching device, it was limited by the control logic circuit and there is no good way to solve it but you can try to connect some serial diodes with the load to decrease the bad effects. But this will lead to bad efficiency.
BR
Sean
Hi Sean:
I tried to increase output capacitor.But it can't improve the output current regulation:LineRegulation.xlsx
If you have other advice,please tell me.
Thanks for the advice.
B/R
Hi gz wu,
Thanks for your feedback, but we are really sorry that we also don't have many more suggestions for your requirement.
BR
Sean