Hi Team,
I am looking for a chip-level solution for a 4 cell Li-ion 18650 battery pack.
The device must include overcharging protection and over-discharge protection and the following features
The number of series cells 4.
Effective voltage 4*4.2V=16.8V
Cell balancing
Undervoltage protection
Overvoltage protection
Stand-alone devices will be more appreciable.
I think a single chip alone cannot make this all possible.
But I believe TI do have some solutions for the same
We are okay if the cell monitoring chip is able to make and break the connection to the charger as well as to the load if over voltage or under voltage is detected, and another chip to charge the battery pack.
Looking forward to your valuable reply