Dear Team,
Here is Kevin from the Delta Taiwan team.
The customer is looking for a suitable LED controller, not sure if we have a suitable device
Vin: 150Vdc ~ 180Vdc,
Vout: 121Vdc ~ 45Vdc
Iout = 0 A~ 3.2 A with 2% tolerance (The current can be adjusted in 255 steps; 12.55mA / Step)
BR
Kevin