This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3445: Suitable device to control current value

Part Number: LM3445

Dear Team,

Here is Kevin from the Delta Taiwan team.

The customer is looking for a suitable LED controller, not sure if we have a suitable device

Vin: 150Vdc ~ 180Vdc,
Vout: 121Vdc ~ 45Vdc
Iout = 0 A~ 3.2 A with 2% tolerance (The current can be adjusted in 255 steps; 12.55mA / Step)

BR

Kevin