Hello,
I have been using the bq27520-G4 in one of our products for several years now (so have experience with the software/tools/processes).
I am now designing a new product and would appreciate some advice on the best fuel gauge chips to meet our needs.
New product information.
a) It couldn't enter relaxation mode because full charge and end-of-discharge conditions without requiring battery relaxation.
b) It may use external charger so it may not enter charge mode.
c) It may use different batteries.
I think that (a) can solve Fast Qmax function.
But I don't have any idea for (b) and (c).
So please answer me some specific questions.
1.If I use an external charger, it can read the accurate RM value?
2.Is there a way to improve the accuracy of the RM value when using it like (b) or (c)?
Shun.