Other Parts Discussed in Thread: UCC27523
Hi team,
My customer is using UCC27537. The schematic is as below: VDD=12V, EN is floating and IN+ is from a opto-coupler.
We found that:
1. When we remove R6 and measure opto-coupler output Pin7, the voltage of Pin7 is a 12V/0V square wave
2. When we soldered R6 to connect opto-coupler Pin7 to UCC27537 IN+, in theory, UCC27537 IN+ should also have a 12V/0V square wave. But we found that the 12V signal is pulled down to some lower voltage.
So could you please help check if this is a normal status? What is the input impedance of UCC27537 IN+ pin and will it draw some large input current at IN+ pin? Thanks.
Best regards,
Wayne