Other Parts Discussed in Thread: TPS92691, LM3492, TPS92692
Hi TI Support team,
CTM use LM3492HC for they UVC LED application. The block diagram will be like this:
UVC LED performance are shown as below:
VF(typ.) = 6.5V @ 0.25A
The following is CTM design calculation process for your reference.
Please help review the schematic, if you have any concern just let me know.
▪ VIN(min.) = 20V, VIN(max.) = 30V
▪ VF(typ.) = 6.5V @ 0.25A
▪ VIOUT(min) = 1.25V
→ VOUT(nom.) = 8 x VF(typ.) + VIOUT(min) = 53.25V
▪ VOUT(max.) = 62.63V @ VFB(max.) = 2.88V
▪ VFB(nom.) = 2.448V @ VOUT(nom.) = 53.25V
→ RFB1 = 332KOhm, RFB2 = 16KOhm
▪ VIN(min.) = 20V, VIN(max.) = 30V
▪ FSW = 900KHz, RRT = 100KOhm
▪ VIN(max.) = 30V, ILED = 0.25A, VOUT(nom.) = 53.25V
→ IIN(min.) = [VOUT(nom.) x ILED]/VIN(max.)
= 0.44375A
→ tON = [1 - VIN(max.)/VOUT(nom.)]/ FSW
= 0.49µs
→ L = VIN(max.) x tON/ 2 x IIN(min.)
= 16.5µH
▪ RIREF = 4.99KOhm @ 0.25A