Other Parts Discussed in Thread: TPS65135
Hi, I am using TPS65131 for the generation of +3.3V and -3.3V from input voltage 2.7V to 5.1V. I followed design example as shared in the datasheet. But the output voltage is not regulating properly. I am hereby attaching my design. I changed C201 to 30pF, C206 to 22pF and C210 to 4.7nF. Kindly suggest the modification, it is very urgent