This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV758P: Vih of the Enable Pin

Part Number: TLV758P
Other Parts Discussed in Thread: ABS

Hi,

We are considering TLV75801PDBVT for out design.

The input voltage of the LDO is 2.2V and enable pin voltage is 3.3V.

Is t possible to connect 3.3V to enable pin when Vin is 2.2V ??

I could not able to see the Vih voltage in the datasheet. Please refer the below schematics and let me know your comments on this.

Thanks and Regards,

Arumugam.P

  • Hello,

    If I am understanding correctly, you are asking if it is okay that VEN > VIN? If that is the case, the answer if yes, this is not a problem. Sometimes the EN pin is related to VIN but it will be noted in the abs max table if that is the case. 

    Best regards,

    Nick