Part Number: BQ24295
Hi Team,
We've received a report from a customer about BQ24295 failure. According to the customer, they have a device which uses a 5000mAh battery and a 3A USB charger adapter has been used to charge the battery through BQ24295. The IC is connected to a microcontroller through I2C. All the registers are configured properly for the IC to work as required. They are observing IC failure many times and when replaced with a new one, the device works fine.
Also, during failure, sometimes the IC detects when a battery is connected (discharge mode) but could not detect when the USB is also connected (charge mode). What could be the cause of the failure.
Regards,
Danilo